AXIS#.MOTOR.LQLL

Description

This parameter is the motor line-to-line quadrature (torque producing) axis inductance.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mH

Range

1 to 232 mH

Default Value

4

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.LQLL

500bh

14h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.LQLL

510bh

14h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6209

1

6209 (0x1841)

AXIS1.MOTOR.LQLL

Unsigned32

Read Only

Yes

71745

2

6209 (0x1841)

AXIS2.MOTOR.LQLL

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.LQLL

6209

Float

Read Only

-